Technical FAQs

Ask a Question

Are the ACSC condenser fans always on? Are they variable speed?

Issue:
Are the condenser fans always on? Are they variable speed? 
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
The condenser fans operate whenever the compressor is operating, otherwise they are off. They are continuously variable speed from 100% down to 30% in order to maintain a 425 psig refrigerant discharge pressure.
Was this helpful?
What can we do to improve the information ?