AUSTRALIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
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
Data Center Assessment Services
Install
Installation Services
Project Management
Operate
Remote Monitoring Services
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
EcoStruxure Asset Advisor
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
AUSTRALIA - Choose Country or Region
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
Presets overwritten when more than one NetBotz appliance monitors a Pelco Camera
Issue:
When more than one NetBotz appliance monitors the same Pelco camera, Pelco camera presets can be overwritten.
Product Line:
NetBotz, Pelco
Environment:
NetBotz software Interfaces
Cause:
The NetBotz appliance sets presets using the default pointer on the camera, “Preset 1”.
Users are allowed to discover the same Pelco camera on more than one NetBotz appliance. No warning message is displayed.
Resolution:
Users should not discover the same Pelco camera on more than one NetBotz appliance.