Technical FAQs

Ask a Question

Can I disable the vodeo from a Camera via Netbotz software?

Issue:

How to disable the video from a Camera via Netbotz software

Product Line:

NetBotz

Environment:

NetBotz version 2 and 3

Cause:

Alternative configurations.

Resolution:

For all NetBotz monitoring appliances the camera can be turned off completely via software configuration under the Advanced View. Choose the Camera Pods applet and settings. Uncheck the option for "Enable video from camera".
 
Was this helpful?
What can we do to improve the information ?