Technical FAQs

Ask a Question

Sun Microsystems Compatibility with Netbotz Advanced Device Crawlers

Issue:
Sun Microsystems Compatibility with Netbotz Advanced Device Crawlers

Product Line:
NetBotz

Environment:
NetBotz v2
NetBotz Device Monitoring Pack (license)

Cause:
Available SNMP information

Resolution:

The NetBotz Advanced Device Crawlers are compatible with the Sun Microsystems Netra servers and the Enterprise 10k.

As of the time the DDFs for version 2 devices were made, the Sun Ultra servers did not report temperature, power supply status, etc by default through their MIB.
Was this helpful?
What can we do to improve the information ?