Technical FAQs

Ask a Question

How do I change User Password settings on Symmetra PX 250/500

Issue:
How to edit User Password settings via system display

Product line:
Symmetra PX 250-500

Environment:
All Product models, all serial numbers

Cause:
How do I change User Password settings on Symmetra PX 250-500

Resolution:
Begin at the home screen of the UPS



Press the wrench key at the lower left of the screen
Select Configuration, then select User configuration



Enter the User password (apc by default)



Select Password settings
Change the password and select apply



The following video demonstrates how the manage user password settings on the Symmetra PX 250/500 Data Center 3 Phase UPS.

Was this helpful?
What can we do to improve the information ?