Technical FAQs

Ask a Question

How do I adjust thresholds for a Netbotz within Advance View?

Issue:

How do I adjust thresholds for a Netbotz within Advance View?

Product Line:

Netbotz Appliance series 300 or higher

Environment:

Netbotz Appliance Version

Cause:

From time to time predefined or custom thresholds may need to be adjusted to allow prevent unnecessary notification due to changes with the data centers environmental controls. This article will explain the necessary step to need to adjust predefined thresholds on a Netbotz Appliance using Advance View.

Resolution:

To be able to configure a Netbotz Appliances predefined threshold we will need Advance View. To download the latest version of Advance View please see Knowledge base FA230223 for links to download the latest version. Once Advance View is installed and you have successfully logged into the appliance, please follow the steps below. In the example below we will adjust the predefine temperature threshold for a probe that is directly connected to the main appliance.
1. Click on the Configuration Icon located between History View and About
2. Locate and double click on Sensor Pods
3. Select Sensor Pod (integrated)
4. Click on Sensor located at the bottom of the window
5. Select the Temperature Sensor
6. Select the Default Range Threshold
7. Click on Edit located at the bottom of the window
8. Adjust the threshold to fit your needs
9. To accept changes continue pressing OK until you have reach the main Window of Advance View

You can repeat these steps as many times required to adjust all the different sensors that are installed on the Netbotz Appliance.
 
Was this helpful?
What can we do to improve the information ?