Technical FAQs

Ask a Question

StruxureWare Operation server is running low of storage space.

 

Issue:

StruxureWare Operation server is running low of storage space.

Product Line:

StruxureWare Data Center Operation

Environment:

StruxureWare Data Center Operation All Versions

Cause:

Server does not have enough storage space to either run another backup or Operation services will not start because of backup or old data and jobs.

Resolution:

The best option would be to increase the storage size for the virtual machine hard drives. To temporally increase available space on the hard drives, Operation has a build in service to purge old data, files and jobs. Console into the server and run

sudo service operations purge

It is also recommended that old backups are manually move or delete backups from the /data/backup directory. To manually delete old backups navigate to /data/backup from the root directory. Then run

rm <filename>

 
Was this helpful?
What can we do to improve the information ?