How deep must the AR7580A Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?
Issue:
Need to make sure the cable cover opens far enough to install and maintain cables.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Customer needs to be able to fully open the hinged cable cover to add, move or change cables.
Resolution:
The AR7580A cable manager needs to be installed at least 10.5" deep in order for the AR7581A hinged cover to open a full 90 degrees.
Also see attached file for photo.