Technical FAQs

Ask a Question

Time Out error when using Netbotz Webservices API

Issue:
Time Out error when using Netbotz Webservices API

Product Line:
NetBotz

Environment:
NetBotz web API

Cause:
Configuration/compatibility

Resolution:
We have seen in some instances when using Netbotz Webservices API and the latest .NET that an application may time out. In such cases, the following setting should be made to .NET:
System.Net.ServicePointManager.Expect100Continue = false;
 
Was this helpful?
What can we do to improve the information ?