Technical FAQs

Ask a Question

Change Temperature Unit of Measure from Celsius to Fahrenheit.

Issue:
Change Temperature Unit of Measure from Celsius to Fahrenheit on a version 2 NetBotz appliance.

Product Line:
NetBotz

Environment:

NetBotz Version 2

Cause:

Temperature scale configuration

Resolution:

The following outlines how to change the temperature unit of measure (Celsius to Fahrenheit or vice versa)for Version 2 Appliances and the Advanced View version 2.x

1. Change the regions settings in Advanced View to the appropriate region.
2. Ensure that the correct time zone is selected on the PC that is running the Advanced View. These changes are made via the Windows Control Panel.
3. Ensure that the Regional Settings are correctly configured on the PC that is running the Advanced View. These changes are made via the Windows Control Panel.

Please be aware that the settings for Celsius or Fahrenheit are not actually set on the appliance, but rather the advanced view software determines the operating system preference by region and reflects that option.
Was this helpful?
What can we do to improve the information ?