Technical FAQs

Ask a Question

Video: Symmetra LX Module Replacement Procedure

Issue
I need to install or replace a module in my Symmetra LX UPS system.  How do I do this?

Product Line
Symmetra LX

Environment
All serial ranges

Cause
Symmetra UPS are designed with modularity so that modules can be added or replaced as needed.  This document contains a video to aid the user in performing the installation of a new module or replacement of an existing module.

Resolution

The following video details the process of replacing the Intelligence, Battery, and Power Modules in the Symmetra LX UPS.

Was this helpful?
What can we do to improve the information ?