Technical FAQs

Ask a Question

SUVT/AIS3000 Dual Mains

"Yes. The SUVT and the AIS3000 can be used with dual mains connection.
One main will go to the normal Input while the another secondary main will be connected to the Maintenance Bypass. (See SUVT/AIS3000 Installation Manual)

"
Was this helpful?
What can we do to improve the information ?