Technical FAQs

Ask a Question

Discontinuation of Replacement Battery Cartridge 44 (RBC44)

Issue:
Discontinuation of Replacement Battery Cartridge 44 (RBC44)

Product Line:
Smart-UPS "SURT" models,  3Kva and larger
(Includes "SURT192" external battery packs)

Environment:
All models, All Serial Numbers

Cause:
APC by Schneider Electric announces the discontinuation of the Replacement Battery Cartridge 44 (RBC44) and its replacement by the new APCRBC140

Resolution:
We will have both APCRBC140 and RBC44 available until we run out of RBC44 stock

The APCRBC140 is backwards compatible with the Smart-UPS On-Line SURT & SURTD products from 3kVA to 20kVA, as well as the New Generation SRT products from 5kVA and upwards.

Note: You can not use the legacy RBC44 product in our New Generation SRT products.
Was this helpful?
What can we do to improve the information ?