Can the center dividing section of the NetShelter SX Colocation be removed?
Issue:
Customers may want to remove the center divider in the NetShelter SX Colocation cabinet.
Product Line:
NetShelter SX Colocation
Environment:
All versions and serial ranges.
Cause:
For various reasons, including the want to mount a particular 0U PDU, customers may wish to remove the center divider of the cabinet.
Resolution:
The center divider of the NetShelter SX Colocation cabinet is not user removable. The divider separates the two sections of the cabinet for security purposes so it's not removable.