Technical FAQs

Ask a Question

Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?

Customers may want to mount a PDU on the accessory channel behind the vertical cable manager.

Product Line:
NetShelter SX

AR7721, AR7722, AR7723

The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.

The vertical cable manager can be installed in the rear-most facing position so that a PDU can be mounted behind it.
Was this helpful?
What can we do to improve the information ?