Technical FAQs

Ask a Question

How to adjust the Contrast on the DG5 display

Issue:
How to adjust the Contrast on the DG5 display  

Product line:
DataGuard 5 Displays  

Environment:
All Airflow units with DG5 board and Display  

Cause:
Text on the Screen is too dark or to light to read 

Resolution:
Dismount the display and turn it over to face the back side.  There will be a small hole in the upper right hand corner.  Using a small flathead screwdriver you can turn the dial to the right to brighten the display and to the left to make it darker.  

 

 
 

 

Was this helpful?
What can we do to improve the information ?