Technical FAQs

Ask a Question

What is the NTP polling cycle used in StruxureWare Data Center Expert?

Issue:

What is the NTP polling cycle used in StruxureWare Data Center Expert?

Product Line:

InfraStruxure Central
StruxureWare Data Center Expert

Environment:

InfraStruxure Central / StruxureWare Data Center Expert any version with NTP client enabled.

Cause:

Default communications timing.

Resolution:

When NTP is enabled, the polling interval is automatically controlled by the NTP daemon and can vary between 64 and 1024 seconds.
 
Was this helpful?
What can we do to improve the information ?