Why do device menus not display as expected when launched from StruxureWare Data Center Expert?
Issue:
When the device user interface is launched from StruxureWare Data Center Expert, menus in the device UI are not displayed as expected
Product Line:
StruxureWare Data Center Expert
Environment:
Microsoft Internet Explorer 6
StruxureWare Data Center Expert version 7.x
Cause:
This issue is known to occur when IE6 is set as the default browser. StruxureWare Data Center Expert does not support IE 6. Although IE 7 is not known to exhibit display issues, it is no longer supported.
Resolution:
Upgrade the default browser on your computer. Supported browsers are:
• Microsoft Internet Explorer® 8, 9, 10
• Mozilla® Firefox® 17.0
• Google Chrome™ 23.0