StruxureWare Central Virtual Machine End User license agreement may be too large for some resolutions using VM Player
Issue:
StruxureWare Central Virtual Machine End User license agreement may be too large for some resolutions using VM Player
Product Line:
StruxureWare Central
StruxureWare Data Center Expert
Environment:
StruxureWare Central version 7.x
Cause:
Undocumented.
Resolution:
StruxureWare Central version 7 has the option to be installed as a VM. Only VMWare ESXi 4.1 is officially supported and this issue has not been seen on version 4.1. If you are trying to install this on VM Player 4.0 you may not be able to see the button to accept the EULA. Simply hitting the enter button on that screen should cause the EULA to be accepted.
To read the full EULA, please see the attached file.