Netbotz 500, 420, or 320 loses configuration when it is rebooted.
Issue:
Netbotz 500, 420, or 320 loses configuration when it is rebooted
Product Line:
NetBotz
Environment:
Version 2 NetBotz
Cause:
Due to a change on the Netbotz devices, some 500s, 420s, and 320s made in mid 2007 began losing some configuration when the system was rebooted. Prior to rebooting the device, the unit would function normally.