Details Returned from NetBotz Devices via Advanced Device Crawlers
Issue:
Details Returned from NetBotz Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for NetBotz appliances assuming the NetBotz DDF (Device Definition File) is installed on the server appliance and the client appliance is SNMP enabled. Please note that not all information listed below is available on all NetBotz models.