Technical FAQs

Ask a Question

Ping Response (ICMP Requests) Can Be Disabled on NetBotz Version 2 Appliances

Issue:

Ping Response (ICMP Requests) Can Be Disabled on NetBotz Version 2 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

Alternative configurations

Resolution:

It is possible to turn off or disable ICMP responses/requests on NetBotz version 2 Appliances (Models 320, 420, & 500). To do so, you must enable "IP Filter" functionality via the Advanced View. Once IP Filtering is enabled, the bot will only respond to requests (including ICMP requests) from specific IP addresses
 
Was this helpful?
What can we do to improve the information ?