Technical FAQs

Ask a Question

Setup Tips for Version 2 Appliances


Setup Tips for Version 2 Appliances

Product Line:



NetBotz version 2


Congifuration suggestions


* Ensure that Network Interfaces and DNS information is complete and correct
* Ensure the Region and Clock settings are complete and correct
* Upgrade the appliance to the latest available version of firmware / BotzWare
* Provide descriptive / unique name for the appliance in the Location configuration
* Change Camera Visual Mode to Widescreen
* Configure the Email Server settings
* Change the NetBotz User password
* Change the Root User password
* Configure sensor thresholds
* Configure camera capture settings
* Configure alert actions
* Test alert actions
* Backup the appliance configuration 
Was this helpful?
What can we do to improve the information ?