Technical FAQs

Ask a Question

How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?

Issue:
 
Upon launching the StruxureWare Data Center Expert client an error message appears stating “Failed to create java virtual machine.”
 
Product Line:
 
StruxureWare Data Center Expert
 
Environment:
 
StruxureWare Client potentially any version.
 
Cause:
 
StruxureWare may be attempting to use a different version of Java on the operating system with which it may not be fully compatible.
 
Resolution:
 
1) Navigate to the Installation directory for StruxureWare Data Center Expert.  (default directory is: C:\Program Files (x86)\StruxureWare Data Center Expert X.X.X)

2) Navigate into the dcexpert directory and open the DataCenterExpert.ini configuration file in a text editor such as notepad.

3) Within the dcexpert directory open the jre directory and then the bin directory.  You will see a javaw.exe file to which you will need to obtain the full path for the next step.

4) Edit the DataCenterExpert.ini file and change it's first line from -vmargs to -vm “fullpath of javaw.exe”
For Example with a 7.2.7 DCE client, instead of reading:
-vmargs
The first line should now read:
-vm "C:\Program Files (x86)\StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe"

5) Save the file and open the client.

6 )If the issue still persists, please contact your local technical support.
Was this helpful?
What can we do to improve the information ?