Can I connect the condenser ducts of an ACSC1XX unit directly outside?
Issue:
Can I connect the condenser ducts directly outside?
Product line:
ACSC1XX
Environment:
All Serial Numbers
Cause:
FAQ
Resolution:
Yes, with certain exceptions. The SC condenser cannot tolerate inlet air below 32 F (0 C), so the unit will have problems during the winter in many parts of the world. Also, the condenser cannot tolerate inlet air hotter than 105 F (40 C). It may be easier to only exhaust the hot air outside and draw the condenser inlet air from the room. Contact your Config Team rep or Systems Engineer for additional assistance.