Technical FAQs

Ask a Question

What is the transfer time of the Back-UPS?

Issue:

What is the transfer time of the Back-UPS?

Product Line:

Back-UPS, Back-UPS PRO

Environment:

N/A

Cause Resolution:

Tranfer time refers to the duration in time it takes the UPS to switch from one state (i.e. Onbattery, Online...) to another.

The transfer time of the BK CS and ES units is 10-12 milliseconds.
The transfer time of the BK RS units is 6-8 milliseconds.
 
Was this helpful?
What can we do to improve the information ?