Technical FAQs

Ask a Question

How to calibrate sensors on version 2 NetBotz appliances?

Calibrating Sensors on NetBotz version 2 Appliances

Product Line:

Version 2 NetBotz sensors

Questionable readings from sensors may suggest that devices require calibration.

As a general rule, sensors (temperature, humidity, and airflow) on version 2 NetBotz Appliances DO NOT need to be calibrated. All of the electronics sensors used by NetBotz appliances are fully calibrated by the supplier.

Please remember the temperature readings have a 1.8 to 3.6 degree F (1 degree C to 2 degrees C) accuracy range depending on the model. Humidity sensor accuracy ranges from 5% to 10% depending on the model.

If you feel your appliance is not accurately reporting temperature and humidity readings correctly, please contact NetBotz Support.
Was this helpful?
What can we do to improve the information ?