Technical FAQs

Ask a Question

NetBotz v3 | Can an Advanced Software Pack be transferred to a different NetBotz appliance?

Issue:
Can an Advanced Software Pack be transferred to a different NetBotz Appliance?

Product Line:
NetBotz v3 Wall Appliance: 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1)

Environment:
NetBotz v3 (all versions)

Cause:
A new NetBotz appliance was purchased and the old one had an Advanced Software Pack associted to it.

Resolution:

The Advanced Software Pack License is tied to the first NetBotz unit it is assigned to.  It cannot be transferred.  For each new NetBotz unit purchased, an Advanced Software Pack License will also need to be purchased. 

NOTE: If the NetBotz Appliance was replaced by technical support due to hardware failure, a replacement Advanced Software Pack can be associated to the replacement appliance.
Was this helpful?
What can we do to improve the information ?