Technical FAQs

Ask a Question

What is the weight capacity of NetShelter open frame racks: AR201, AR203A and AR204A?

Issue: 
Static load rating is required. 

Product Line: 
NetShelter Open Frame Racks

Environment: 
All models, all serial numbers. 

Cause: 
On the APC website, weight capacity is not noted in the Specifications tab of the product pages.  

Resolution: 
AR203A and AR204A Weight Capacity 2,000 lb (907.18 kg).  
AR201 Weight Capacity 1,000 lb. (453.6 kg). 
Was this helpful?
What can we do to improve the information ?