Technical FAQs

Ask a Question

Data Center Expert | Where can I find the serial number and MAC address?

Issue:
Unable to locate the serial number or MAC address of the Data Center Expert appliance.

Product Line:
StruxureWare Data Center Expert (DCE)

Environment:
Struxureware Data Center Expert (all versions)

Resolution:

Physical Data Center Expert Appliance

Serial Number: Printed on a white sticker along with the model number and associated barcodes.  The format of the serial number will be FAXXXXXXXXX.
MAC Address: Within the Data Center Expert desktop client, click on the "Help" menu and select "About StruxureWare Data Center Expert."

Virtual Data Center Expert Appliance
Serial Number: Printed on the white envelope that your passcode came in.  If a DIGI SKU was purchased, the serial number will be the passcode for the Virtual Machine Activation Key.
Alternative Serial Number: Within the Data Center Expert desktop client, click on the "Help" menu and select "About StruxureWare Data Center Expert."
MAC Address: Within the Data Center Expert desktop client, click on the "Help" menu and select "About StruxureWare Data Center Expert."
Was this helpful?
What can we do to improve the information ?