Technical FAQs

Ask a Question

Video: How to view event logs on an InRow ACRD200 cooling system

Issue:
How View Event Logs on an ACRD200 Cooling Unit

Product line: 
InRow Cooling Products ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:
 


First you need to access the View Event Logs menu you can do this by hitting the <ESC> until visible
 
Then select ENTER
 
Now you can use the Up or Down arrows to scroll through the events
 
Was this helpful?
What can we do to improve the information ?