Technical FAQs

Ask a Question

What accessories are available for AR3100X717 or AR3104X717?

Issue:
Customer is in need of accessories for AR3100X717 or AR3104X717.

Product Line:
NetShelter Dell OEM

Environment:
All versions and serial ranges.

Cause:
Need to identify compatible accessories.

Resolution:
All accessories that are compatible with AR3100 and AR3104 also compatible with AR3100X717 and AR3104X717 with one exception AR7719, Castor Kit. For a list of the available accessories please see the NetShelter Accessory Compatibility Chart which is available from the Knowledge Base on the APC website. Please search for document FA158651: http://www.apc.com/site/support/index.cfm/faq/ 

Was this helpful?
What can we do to improve the information ?