Technical FAQs

Ask a Question

Is the ACSC fan system fault tolerant?

Is the ACSC fan system fault tolerant? 
Product line:
ACSC100, ACSC101
InRow Cooling
Yes, there are 2 power supplies in the unit for the condenser and evaporator fans. If 1 fails the other can supply 70% of the maximum power needed, so maximum fan capacity would be reduced approximately 30%. They are hot swappable as well; a user can replace the failed power supply from the front of the unit while the ACSC is still in operation. The evaporator fans are also hot swappable.
Was this helpful?
What can we do to improve the information ?