Technical FAQs

Ask a Question

What is the Thermal Capacity of the NetShelter CX Mini and CX2?

Issue:
Define the thermal capacity of the NetShelter CX.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Know the thermal capacity so that it's not exceeded.
 
Resolution:  
AR4000MV NetShelter CX Mini = 800W
AR4018A / AR4018IA NetShelter CX 18U = 1.2kW
AR4024A / AR4024IA NetShelter CX 24U = 2.4kW
AR4038A / AR4038IA NetShelter CX 38U = 3.6kW.
Calculate the internal load by adding together the power ratings of the installed equipment.
 
Was this helpful?
What can we do to improve the information ?