Technical FAQs
Technical FAQs
Issue:
What are the lengths of the DC cables that are attached to single phase Symmetra extended run (XR) frames?
Product Line:
Single Phase Symmetra XR Frames
Environment:
All serial ranges
Cause:
These products are designed to be able to reach each other if position in the same area. This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
Resolution:
The following table outlines the cable lengths of the DC cable provided with each of the single-phase Symmetra Extended Run cabinets.
XR Type |
Cable Type and Length |
SYXR4 |
Fixed or Detachable 5ft (1.5m) |
SYXR12 |
Fixed or Detachable 5ft (1.5m) |
SYRMXR4 |
Fixed 2ft (0.6m) |
SYARMXR3 |
Fixed 3.5ft (1.0m) |
SYARMXR9 |
Fixed 5ft (1.5m) |
SYAXR9 |
Fixed 5ft (1.5m) |