Technical FAQs

Ask a Question

Can the side slam latches of a NetShelter SX cabinet be locked or disabled so they can only be opened from inside the cabinet?

Issue: 
The NetShelter SX has side slam latches that unlock from outside the cabinet. 

Product Line: 
NetShelter SX

Environment: 
All models, all serial numbers. 

Cause: 
A concern for security would most likely create the need to 'freeze' the side locks. 

Resolution: 

See attachment below. 
Was this helpful?
What can we do to improve the information ?