Technical FAQs

Ask a Question

INTERNAL: How to install a Luvata Flooded Receiver Package on a Uniflair or InRow cooling unit

INTERNAL 
 
Issue:
How to install a Luvata Flooded Receiver Package on a Uniflair or InRow cooling unit
 
Product line:
Uniflair, ACRD600, ACRD601, ACRD600P, ACRD601P
 
Environment:
All Serial Numbers
 
Cause:  
Install, Repair
 
Resolution: 
 
Low Temperature Kit Unpacking
 
NAM-ASME (ACAC75014) versions
 
1. Remove plywood top and sides from the pallet.

 
2. Remove the valve box (contains safety valve, ball valve, head pressure valve, and check valve).
3. Remove brackets.

4. Remove receiver kit.

 
 
Install kit inventory
 
NAM-ASME (ACAC75014) versions

 

 
NAM-ASME (ACAC75014) versions
 
1. Install the bracket using the 1/4 in. washers and 1/4 in. bolts.

2. Install the safety valve onto the receiver kit. Use thread sealing adhesives or raw adhesive tape as necessary.
3. Install receiver kit using the M10 washers, M10 bolts, and M10 nuts.

 
4. Install included valve and pipes to the inlet and outlet connections on the condenser.

 
NAM-ASME (ACAC75014) versions

 
Was this helpful?
What can we do to improve the information ?