Technical FAQs

Ask a Question

Does the NetShelter WX castor kit AR8359 fit onto the AR106, AR109 or AR112.

Issue:
There does not appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
Customer wants to add castors to AR106, AR109 or AR112.

Resolution:
There is no castor kit for the AR106, AR109 or AR112.
The smallest cabinet that has a castor kit available is the AR100  and AR100HD. They have AR8359 available as a castor kit.
Was this helpful?
What can we do to improve the information ?