Technical FAQs

Ask a Question

Video: Data Center Expert | How do I configure auto-login when launching to APC devices?

Issue: 
How do I configure auto-login when launching to APC devices within the StruxureWare Data Center Expert desktop client?

Product Line: 
- InfraStruxure Central (ISXC)
- StruxureWare Central (SWC)
- StruxureWare Data Center Expert (DCE)

Environment: 
- ISXC, SWC, & DCE (all versions)
- APC Network Management Cards (NMC)

Cause: 
Double clicking on an APC device (NMC) in StruxureWare DCE launches a browser window to that device automatically logging in if configured correctly.

Resolution: 



1) Open the DCE desktop client and navigate to: Monitoring perspective > Device View pane.
2) Right-click on an APC device and select Device Launch settings.
3) Ensure that the correct protocol, port, username, and password are defined for accessing the devices web interface.  Select OK.
4) Double-click on the device, or right-click and select Launch to Device, and the web interface of the device should load and automatically log in.
Was this helpful?
What can we do to improve the information ?