Technical FAQs

Ask a Question

Can the NetShelter cabinet lay flat during shipment?

Issue:
Customer is asking if the NetShelter cabinet may be tilted or lay flat on it's side.

Product Line:
NetShelter SX, NetShelter SV, NetShelter VX, NetShelter AV

Environment:
All versions and serial ranges.

Cause:
In order to save space, or fit into an oddly shaped freight container (like an air freight container), someone may wish to lay the NetShelter cabinet flat.

Resolution:
Absolutely not. A NetShelter cabinet is never to be tilted or laid flat during transit. 
The only exception is the AR2400FP1 which ships unassembled, and can lie flat during transport. 
Was this helpful?
What can we do to improve the information ?