Issue:
Can I run cables over the SC? If so, how many?
Product line:
ACSC1XX
Environment:
All Serial Numbers
Cause:
FAQ
Resolution:
Yes, there is a cable support bridge trough available as an accessory (ACAC10021). You will need (2) per SC unit to carry
both data and power cables across the unit. Approximately 80 CAT5 cables or 8 power whips fit into a trough.