Technical FAQs

Ask a Question

Can I power the ACSC1XX unit from a UPS


                                                                                                                                                       
Issue:  
Can I power the ACSC1XX unit from a UPS

Product line:
ACSC1XX

Environment:  
All Serial Numbers

Cause:
FAQ

Resolution:
 
The SC should be powered from a dedicated circuit; the unit has very high in-rush current (>55 amps) that may overload the UPS every time the compressor turns on. If you must power the SC from a UPS, then it needs to be properly sized; a dedicated UPS would be preferred. Contact your Config team rep or Systems Engineer for additional assistance.
 
 
 
Was this helpful?
What can we do to improve the information ?