Technical FAQs

Ask a Question

Can the NetShelter shock pallet be reused?

Issue:
Customers ask to reuse a NetShelter shock pallet after it' ship a cabinet with equipment installed.
 
Product Line:
NetShelter SX
 
Environment:
All models and serial ranges
 
 
Cause:
Customers may want to use the pallet to make multiple shipments. 
 
Resolution :
The NetShelter shock pallet is designed for a single use only. Please do not reuse the shock pallet after the first shipment with equipment installed.
Was this helpful?
What can we do to improve the information ?