Technical FAQs

Ask a Question

Where are your TechCool manuals?

Issue:
Where are your TechCool manuals?
 
Product line:
Airflow TechCool Units
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
The TechCool (TC) product line (purchased from The Airflow Company) has been discontinued and is not featured on our website as a current product.  Below you will find archived TC manuals that should be able to assist you.  If you require more assistance, please call our technical support office at 888-695-6500.

NOTE:
WEST KINGSTON, R.I. - October 23, 2000 - American Power Conversion (NASDAQ: APCC) announced acquisition of privately held Airflow Company, a leading precision cooling equipment manufacturer.
Airflow’s product line included floor and ceiling-mounted precision cooling systems as well as management systems used in a variety of applications including datacenters, co-location facilities and telecommunication stations. Airflow was recognized throughout the industry for its highly efficient cooling products, which reduced electricity costs as well as minimize the need for additional equipment to manage humidity levels. Their solutions offered one of the smallest footprints in the industry.
Was this helpful?
What can we do to improve the information ?