On the RP Chilled Water the top piping connections have one pipe for the return plumbed to the top, but no supply pipe connection, is this normal?
Issue:
On the RP Chilled Water the top piping connections have one pipe for the return plumbed to the top, but no supply pipe connection, is this normal?
Product line:
ACRP50x
Environment:
Data Center Cooling
Cause:
Resolution:
Yes this is normal. In the crating of each unit will be two long extension pipes that is field installed and insulated. If you need more clearance, it is suggested to use the flex pipe kit.