Technical FAQs

Ask a Question

Which 0U PDUs can be stacked vertically on the Rear Accessory Rails of a NetShelter cabinet?

Issue:
Customers want to know which PDUs are short enough to stack vertically in a NetShelter cabinet.

Product Line:
NetShelter SX, NetShelter SV,

Environment:
All versions and serial ranges.

Cause:
Some short 0U PDUs cane be installed atop one another on the rear accessory rail, to help save space. This requires a cabinet of 42U height or taller.

Resolution:
This is a list of half-height PDUs that can be installed in pairs, vertically on the rear accessory rail of a NetShelter cabinet:

Basic
AR6002A
AR6003A
AR6007A
AR6009A
AR6015A
AR6020A
AP6031A
AP6037A
AP6039A
AP6201CH
AP6221CH
AP7516
AP7526
AP7580
AP7581
AP7582
AP7583
AP7584
AP7585
AP7586
AP7615
AP9551
AP9567
AP9568
AP9572

Metered
AP7152
AP7155
AP7175
AP7800
​AP7801
​AP7802
​AP7802J
​AP7802BL
​AP7811
​AP7811B
​AP7820
​AP7820B
​AP7821
​AP7821B
​AP7822
​AP7822B
​AP7823
AP8831
AP8833J
AP8859
AP8858NA3
AP8858EU3

Metered 
AP7900
AP7900B
AP7901
AP7901B
AP7902
AP7902B
AP7902J
AP7902BJ
AP7911A
AP7911B
AP7920
AP7920B
AP7921
AP7921B
AP7922B
Was this helpful?
What can we do to improve the information ?