Technical FAQs

Ask a Question

What's the difference between shipping load, dynamic load and static load? How are these ratings calculated?

Issue:
Customers need to know the difference between shipping load, dynamic load and static load ratings, and how they are calculated.

Product Line:
NetShelter SX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers need to make sure the they do not exceed the load capacity of the cabinet during installation, travel or operation. Some may be wondering if they can safely exceed these ratings or recalculate them.
 
Resolution:

Please see attachment.
 
Was this helpful?
What can we do to improve the information ?