Technical FAQs

Ask a Question

Netbotz 500, 420, or 320 loses configuration when it is rebooted.

Issue:

Netbotz 500, 420, or 320 loses configuration when it is rebooted

Product Line:

NetBotz

Environment:

Version 2 NetBotz

Cause:

Due to a change on the Netbotz devices, some 500s, 420s, and 320s made in mid 2007 began losing some configuration when the system was rebooted. Prior to rebooting the device, the unit would function normally.

Resolution:

Version 2.6.2 of Botzware has fixed this issue.

Was this helpful?
What can we do to improve the information ?