AFGHANISTAN - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
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
Data Center Assessment Services
Install
Installation Services
Operate
Remote Monitoring Services
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
AFGHANISTAN - Choose Country or Region
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
What are the potential results of using a Smart-UPS with X-10 equipment?
Issue:
What are the potential results of using a Smart-UPS with X-10 equipment?
Product Line:
Smart-UPS
Environment:
All models, All Serial Numbers
Cause:
Product Information and Application
Resolution:
What is X-10 technology? It is a home control system that sends high frequency
electrical signals that ""piggy-back"" the AC line to control common household
items such as lights and appliances.
The use of such technology does not adversely affect APC UPSs. However, a UPS
or surge suppressor may absorb or filter out X-10 signals as UPSs and
suppressors treat these signals as noise. The result, then, is that some X-10
equipment may cease to receive signals.
A possible solution is to install an X-10 isolator which prevents a UPS from
filtering out these signals. One commercial solution is currently available
from WWW.Smarthome.com. It is called a ""noisy device filter""