Technical FAQs

Ask a Question

Are there any limits to the amount of users that can be added to a version 3 NetBotz appliance?


User amount limits

Product Line:



NetBotz version 3 appliances


NetBotz User names are limited without the advanced software pack


Version 3 NetBotz appliances have a user name creation limit of 5 users. If the NBWN0005 advanced software pack is installed, that is changed to unlimited.

Note that the NBWN0005 is not compatible with the NetBotz NBWL0355 and the NetBotz NBRK0550 and NBRK0570 come with the advanced software pack pre-installed. The only appliances that can use the NBWN0005 are the NBRK0450 and NBWL0455.
Was this helpful?
What can we do to improve the information ?